Wiping the device
Wipe the device before decommissioning it to help prevent potential disclosure of data.
Prerequisites:
- Meter connection using ION Setup.
- Login credentials.
- Security configuration access privileges.
notice
DATA LOSS
Save all important data from the device before performing a reset.
Failure to follow these instructions can result in data loss.
notice
LOSS OF ACCESS
Ensure you maintain sufficient access to communicate with your device.
Failure to follow these instructions can result in loss of access to the device.
Your device might have stored users, passwords, or certificates. Wiping the device in the following order helps ensure that confidential information is not left on the device.
notice
Loss of Confidentiality
| ● | Ensure that you follow all device wiping steps in the order listed. |
| ● | Overwrite the communications module registers last to maintain meter connectivity. |
Failure to follow these instructions can result in loss of confidentiality.
To wipe the device:
- Overwrite the meter template file. This overwrites the meter template with the default factory template. See “Overwriting the Meter template file” for detailed steps.
- Delete files in the documents folder in SFTP file directory using SFTP client software. See “SFTP” for more information.
- Delete the custom SSL certificate. See “Deleting a custom SSL certificate” for more information.
- Delete webpages. See “Deleting custom webpages” for more information.
- Delete the IEC 61850 configuration file. This deactivates functions related to the IEC 61850 protocol. See “Deleting an IEC 61850 configuration file” for more information.
- Restore default security configuration. See “Restoring default security configuration” for more information.
- Overwrite factory module registers. This deletes values
for:
- Device owner.
- Device tag.
- Device location.
- Device name.
See “Overwriting factory module registers” for more information.
- Perform a Master Reset. This deletes values for:
- Event log, data, and waveform records.
- Power quality event (COMTRADE) files.
- Energy, metering, min./max., revenue and test mode, and peak demand values.
- Disturbance (sag/swell event) counter, EN 50160 parameters and statistics.
- Overwrite communications module registers. This deletes values for network infrastructure details. See “Overwriting communications module registers” for more information.