Digital alarms

These alarms are triggered when the associated digital input changes state.

You can configure the alarm to be active when the digital input is on or off, depending on the alarm’s purpose.

For example, if you used a digital input to monitor a breaker that is always supposed to be on, you would set the alarm to be active when the breaker has tripped.

Note: To stop a digital alarm from being displayed, set the alarm priority to Info Only. Disabling the digital alarm will disable all alarming functions of the associated digital input.

For more information see Digital Input Module in ION Reference help.