Enable and configure HSTC alarms

Enable HSTC alarms using ION Setup or the display.

Configure HSTC alarms using ION Setup.

Changing your meter’s HSTC alarm configuration deletes all existing Data set and HSTC waveform logs.

notice

data Loss

Ensure that all important data has been recorded before configuring HSTC alarms.

Failure to follow these instructions can result in data loss.

 

Enabling and configuring HSTC alarms using ION Setup

To enable and configure HSTC alarms using ION Setup:

  1. Open ION Setup and select the Setup Assistant for your meter.
  2. Click Alarming > Transient.
  3. Select High Speed Transient, and then click Edit.
  4. In High Speed Transient Setup, enable or configure the setup registers:
  5. Setup Register Value/Range Description
    Enabled/Disabled Enabled, Disabled Specifies if HS Transient capture is enabled.
    Voltage Reference Ve, Vn Determines the voltage reference. Set the voltage reference to match your system configuration.
    Magnitude Threshold (VRMS) 120–7100 Specifies the absolute voltage threshold that must be exceeded to trigger a HS transient capture.
    Note: This value is entered in RMS volts.
    Duration Threshold (μs) 0–250.0 Specifies the length of time that the magnitude threshold must be exceeded to trigger a HS transient capture. If this register is set to zero, any voltage that exceeds the magnitude threshold will trigger a HS transient capture.
    Alarm Priority None, Info Only, Low, Medium, High Select the alarm priority you want to associate with the HS transient alarms. To stop an alarm from being displayed without affecting other meter features, set the alarm priority to Info Only.
    Custom Priority 0–255 Select custom priority to view and configure the priority associated with the alarm. The event log cutoff value is displayed for reference. Event priorities above the cutoff are stored in the meter’s event log.

  6. Click Save. ION Setup performs a configuration check and displays a message if the Magnitude Threshold setting is below the configured nominal voltage.

Enabling HSTC alarms using the display

To enable and disable HSTC alarms using the display:

  1. Review your meter’s nominal voltage settings.
  2. Set the HSTC magnitude threshold to a value higher than the nominal voltage.

See Disabling and enabling alarms using the display for instructions.