Event log

Your meter records events produced by the meter’s ION modules or external meter events.

Meter events, such as meter configuration or changes to I/O state, have priority values associated with them, so you can control what events are logged. Each event has a priority based on its type and severity, and for most events you can configure the priority. The event log records the date and time of the event, along with relevant details about the event.

Your meter’s event log can be viewed through ION Setup and the display.

For more information on how to view the event log, see Viewing and downloading an event log.