Configuring digital output energy pulsing using ION Setup
You can configure your meter’s onboard digital outputs for energy pulsing using ION Setup.
When configuring your meter, the configuration interface may show all the possible ports, regardless of what is physically available on your meter.
Ensure that the digital output port is available for energy pulsing and not associated with another function.
Note: For applications where accuracy is important, use the digital output located on the meter base.
- Start ION Setup.
- Open the Setup Assistant for your device.
- Select Energy pulsing.
- Select an energy pulsing source tab (such as Wh Del) to configure energy pulsing using your meter’s digital output.
| Parameter | Description |
|---|---|
| Kt | The amount of energy source required to trigger the digital output. For example, in the Wh Del tab, the Kt value would be amount of real energy delivered (Wh Del) per pulse. |
| Pulse Width |
The minimum time in seconds between pulse transitions. |
| OutputMode | Select
the desired output mode:
|
| Port | Select an output port from the list. Only available output ports are shown (ports that are not associated with another function). |
| (energy source) ovrld |
Pulsing normally indicates that the output port should be operating normally. Pulsing suspended indicates that the output port is not able to pulse quickly enough. Modify the Kt value to decrease the number of energy pulses. |
Note: To perform specialized configuration go into the advanced mode of ION Setup and modify or add a new Calibration Pulser module. This is an advanced procedure that should only be performed if you have advanced knowledge of ION and the power system your meter is connected to.
For more information, see Calibration Pulser Module in ION Reference Help.