Advanced security mode
Advanced security mode lets you add up to 50 users, has strong user login, and privilege management.
Note: We recommend that you use Advanced security mode.
This topic lists the advanced mode security capabilities, as well as detailed information on user access permissions, and the default username and password.
Advanced security mode capabilities
The following table lists the security capabilities of advanced security mode:
| Security capability | Description |
|---|---|
| User credentials and password robustness | Use a single account to access the meter with a numeric password for login. |
| Use multiple user accounts with alphanumeric passwords for login and configuration changes. | |
| Use any combination of valid characters, with a maximum length of 16 characters. | |
| Define a minimum password length requirement. | |
| Enforce password character requirements using industry-standard password complexity options. | |
| Password strength feedback using ION Setup. | |
| User account lockouts and timeouts | Define user account lockout criteria after unsuccessful login attempts and define event timeout period. |
| User privileges | User accounts with variable permissions to read access or configuration privileges. |
| Webpages | Disable or enable webpages for viewing meter data online using a web browser (Web Server). |
| Configuration |
Disable or enable ability to configure the meter using:
|
| Disable and enable time synchronization. | |
| Password required for broadcast time synchronization configuration changes using the display or communication protocols. | |
| Cybersecurity event logs and reports |
Set up cybersecurity event logs and alarms using event priorities. |
User access (Advanced security mode only)
The following table lists the Advanced security mode user access details:
| Access type | Permission |
|---|---|
| Time Sync Access | Set the meter’s time and time synchronization parameters. |
| Read Access | View parameters, except security configuration. |
| Peak Demand Reset Access | Reset peak demand values. |
| Comm Config Access | Configure communication settings. |
| Test Mode Access | Switch the meter to test mode, if available with your meter type. |
| Full Meter Config Access | Configure meter settings. |
| Security Config Access | Configure security settings. |
User accounts (Advanced security mode only)
The following table lists the Advanced security mode user account details:
| Username | Default password | Account description | |
|---|---|---|---|
| User1 | 0 (zero) | Default administrator. This account has full meter access, including configuration. | |
| User2 | 0 (zero) | Default viewer. This account has view only access. | |
| User3, User4, ... User50 | - | These user accounts are not activated; they do not have default passwords. | |
Related topics: