Creating and changing user passwords
Create strong passwords for each user that requires access to the meter. Default account settings and weak passwords are often the source of unauthorized access by malicious users.
To optimize cybersecurity in a protected environment, follow user account management tasks as described by your organization or contact your network administrator, for example, maximum password age or history policies.
Prerequisites:
- Open a Security Configuration File in the ION Setup Security wizard.
To change a password:
- In the ION Setup Security wizard, click Next to navigate to Define individual users/passwords.
- For each user that you want to assign or change a password:
- Highlight the USER, and then click Password.
- Enter and confirm the password.
- Click OK.
TIP: Use Password strength to increase the password complexity. A password can be any combination or letters and numbers, up to 16 characters.
- Next, either:
- Continue configuring the meter security settings.
- Click Finish to push your security configuration changes to the meter.
notice
data Loss
Record your device's user and password information in a secure location.
Failure to follow these instructions can result in loss of data.
You can also change the password using ION Setup Diagnostics tool, Security Options Module using ION Setup Advanced Mode, and Power Monitoring Expert.