Editing meter access event logging
The event log monitors meter access events such as user logins and user account lockouts.
You can edit the default meter access event priorities that are logged to the event log to meet your reporting requirements.
To monitor meter access events, see Monitoring the event log.
Prerequisites:
- Open a Security Configuration File in the ION Setup Security wizard.
To configure meter access event logging:
- In the ION Setup Security wizard, click Next to navigate to Select protocol lockout options:
- Click Events. The Event Priorities
dialog box opens:
- For each meter access event priority, set the value according to your reporting requirements. The following table describes the priority value ranges:
- Click OK.
- Next, either:
- Continue configuring the meter security settings.
- Click Finish to push your security configuration changes to the meter.
Priority | Description | Value range |
---|---|---|
None |
Not recorded in the event log. |
0 |
Info Only |
The default event log cutoff value is 5. Event values equal to or less than the cutoff value are not recorded in the event log nor in syslog records. |
1–5 |
Recorded in the event log and in syslog records. |
6–63 |
|
Low |
Produces low alarm. Recorded in the event log and in syslog records. |
64–127 |
Medium |
Produces medium alarm. Recorded in the event log and in syslog records. |
128–191 |
High |
Produces high alarm. Recorded in the event log and in syslog records. |
192–255 |
You can also change event priorities for cybersecurity events using ION Setup Advanced Mode.