Limiting user access

Limit user access to the minimum level of access needed to perform their job functions.

Revoke user privileges when no longer needed due to role change, transfer, or termination. User credentials do not expire.

NOTE: The maximum number of users is 50. Users can be added or removed at any time.

Prerequisites:

To define user access:

  1. In the ION Setup Security wizard, click Next to navigate to Define individual users/passwords.
  2. notice

    data Loss

    Record your device's user and password information in a secure location.

    Failure to follow these instructions can result in loss of data.

     

  3. For each user, select the user, and then assign their permissions:

  4. See for Access information on the device access level permissions.

  5. Next, either: