Rapid Voltage Change
Available on: Advanced and Standard
Rapid Voltage Change (RVC) is a quick transition in RMS voltage between two steady-state conditions, during which the voltage does not exceed the sag/swell thresholds.
You can configure the Sag/Swell module to detect and measure RVC and record the event in the meter’s Event Log.
For more information see Sag/Swell Module in ION Reference help.