Logging overview

The meter’s logging frameworks include factory-configured data recorders, waveform recorders, and event logs.

The logging frameworks store data related to:

  • Power quality and compliance1
  • Energy and demand
  • Revenue metering
  • Trending and forecasting1
  • Meter events

When your system’s nominal parameters are programmed into the meter, power quality events such as sags and swells are automatically detected, and associated voltage and current data and waveforms are logged. Meter data is stored in non-volatile memory, so data is retained even if the meter loses power. If your system nominal values fluctuate, you can configure the meter’s setpoint learning feature to learn your power system’s normal operating values, then use that information to help identify voltage sags and swells.

The meter’s logging framework also supports burst data logging for sag/swell events.1 When burst data logging is enabled, additional data records immediately before and immediately after the sag/swell event are captured. Energy management systems can then retrieve this information for use in applications, such as power event analysis.

Tip: Connect devices directly to an Ethernet network to help maximize the performance of your power management system.

You can also configure the meter to email data from the logging frameworks. For more information, see the PowerLogic MeterM@il Internal Email Client Feature technical note, available on www.se.com.

Meter events are recorded in the meter’s onboard event log. You can also configure the meter to record events to an external syslog server.

For details on how to set up syslog, see Configuring Syslog network settings using ION Setup.

1 Available on: Advanced and Standard