Editing accumulated energy values using ION Setup
You can edit energy values such kWh and kVARh using ION Setup.
Note: Ensure you have recorded accumulated energy values before upgrading your meter’s firmware. You can then re-enter these values after the upgrade.
Note: Revenue-locked meters must be unlocked before accumulated energy values can be edited. See Revenue locking your meter for more information
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Click Template.
- Click the Register Edit tab, click Energy then click Display. Enter
your meter’s password (if prompted) and click OK.
The Register Editor screen displays.
- Click Edit to enable editing.
- Enter values for kWh, kVAh and kVARh as required. Click Send to finish.
Note: Only values that have the check box selected will be sent to the meter.
- Click Close to close the Register Editor screen.