Connecting to an ION device over serial
You can connect to your ION device for the first time and to an existing device over serial.
Connecting to a device for the first time over serial
To connect to a device for the first time over serial:
- On the Home screen, select Connect to devices.
- Under How would you like to connect?:
- Select Serial Connection.
- Enter the Serial Port.
- Enter the Format.
- Enter the Baud rate.
- Enter the Unit ID if you are using a connection that requires an ID.
- Under Connection settings:
- Enter the Hardware profile.
- Enter the Timing profile.
- (Optional) Select Manage timing profiles, and then under ION.SerialConnection enter your Timing profile preferences.
- Select Connect.
-
Enter the device credentials, and then select Authenticate.
- Select Create Project With The Device.
-
If a certificate notification appears, review the message, and then confirm the connection if you trust the certificate.
- After the project is created, select Open project.
Connecting to an existing device over serial
To connect to an existing device over serial:
- On the Home screen, select the device's Project and Site.
- Open the device table of contents.
- Go to the toolbar, and then select Connect.
- Under Connection settings:
- Enter the Hardware profile.
- Enter the Timing profile.
- (Optional) Select Manage timing profiles, and then under ION.SerialConnection enter your Timing profile preferences.
- Select Connect.
-
Enter the device credentials, and then select Authenticate.
If a certificate notification appears, review the message, and then confirm the connection if you trust the certificate.
- Review the connection comparison and then select OK.
Note: When there are detected differences, review them, and then select Associate. This action will overwrite the local device content with the incoming differences from the connected device.