Standards settings
Standards settings
| Parameter | Values | Description |
|---|---|---|
| IEC 61000-4-30 | ||
| IEC 61000-4-30 | On, Off |
Turns on IEC 61000-4-30 calculations. |
| Interruption Threshold | 0–98 |
Enter the voltage level as a percentage of the nominal voltage that triggers an interruption. Note:
|
| Hysteresis Margin | 1–99 |
Enter the level as a percentage above the Interruption Threshold that ends an interruption. Note:
|
| Log 3s Measurements | ON, OFF | Records power quality data every 3 seconds based on IEC 61000-4-30. |
| Log 10s Measurements | ON, OFF | Records power quality data every 10 seconds based on IEC 61000-4-30. |
| Rapid Voltage Change | On, Off |
Turns on rapid voltage change to detect sudden voltage changes. Note: This option is only available when IEC 61000-4-30 is on. |
| Threshold | 1–100 | Enter the change in voltage change as percentage of RMS that triggers a rapid voltage change event. |
| Hysteresis Margin | 1–100 | Enter the voltage level as percentage of RMS that ends a rapid voltage change event. |
| EN 50160 | ||
| EN 50160 | On, Off |
Turns on EN 50160 calculations. |
| Log EN 50160 Measurements | On, Off | Records power quality measurements based on the EN 50160 standard. |
| EN 50160 Reset | NA | Clears the power quality counters and statistics related to the EN 50160 standard. |
| IEEE 519 | ||
| IEEE 519 | On, Off |
Turns on IEEE 519 harmonic limit calculations. Note: PLES does not support IEEE 519 harmonic limit configuration or limit viewing for the ION8650. |
| Harmonic Limits | IEEE Std 519-2014 Edition, IEEE Std 519-2022 Edition |
Choose the standard that you want to use for harmonic limit definitions. Note: The options available depend on your device firmware version. |
| Bus Voltage | 1.0 Kv and below, Above 1.0 kV to 69.0 kV, Above 69.0 kV to 161.0 kV, Above 161.0 kV | Choose the bus voltage definition based on the chosen Harmonic Limits. |
| Maximum Short Circuit Current (Isc) | 1–1000 |
Enter the maximum short circuit current available at the point of common coupling (PCC). |
| Maximum Demand Load Current (Il) | 1–100 | Specifies the highest typical consumption (current) in normal operation. |
| Ratio (Isc/Il) | Isc/Il | The calculated short circuit ratio of the Maximum Short Circuit Current (Isc) and Maximum Demand Load Current (Il). |
| Log Individual Harmonics | On, Off |
Records individual harmonics based on the IEEE 519 standard. Note: This option is only available on devices that support individual harmonics logging. |