Linking data recorder inputs
Use linking to configure data recorder inputs. See Downloading data recorder logs before configuring a data recorder; configuration changes will delete all recorded data.
notice
data Loss
Ensure that all important data is recorded before configuring data recording.
Failure to follow these instructions can result in data loss.
Prerequisites
To link data recorder inputs:
- Select Logging > Data Recorders.
- Go to the data recorder to which you want to add links.
- Under Actions select
to open the Select Input menu. - Go to an available Input that you want to link.
- Under Actions select
to open the Link Parameters menu. - To link a single input:
- Choose the parameter that you want to record and then select Link.
- To link multiple available consecutive inputs:
- Turn on Link Multiple.
- Choose the parameters that you want to record and then select Link.
Note: Link Multiple is only available if there is at least one consecutive available input. For example, if you selected Source 5, and Source 6 and Source 7 were also available, you could turn on Link Multiple and then choose three parameters to link to those inputs.
Tip: Hover over the right side of the Parameters heading and then select
to search for a specific parameter. 
- Select Apply.
- Select Save Working Copy.
- Synchronize changes.
Tip: Turn on Hide Linked Inputs to see only the available data recorder inputs.