Use an E-Mail Action to Enable an Engineer to Acknowledge Alarms Remotely

This example demonstrates how an E-Mail Action might be used to enable an engineer to acknowledge alarms remotely, via e-mail.

Example:

On a particular Geo SCADA Expert system, alarm redirection is used to enable engineers to acknowledge alarms via e-mail.

In order to be able to acknowledge alarms via e-mail:

  • Using an Original WebX client, the engineers need to have their User Accounts configured to allow them to access Geo SCADA Expert via the web:

  • The engineers need to have the required permissions to allow them to acknowledge alarms on the database item(s) for which Geo SCADA Expert is to trigger alarm redirections, see Allocating Security Permissions.
  • If the Area of Interest feature is enabled on the system, the engineers also need to have access to the Area of Interest that is associated with the redirected alarms, see Restrict Alarm and Event Access to Specific Areas of Interest.

An E-Mail Action is configured to redirect alarms to a group of engineers:

The engineers’ User Accounts are each associated with the specified User Group:

The E-Mail Action is configured as the redirection Action on the Forms of those database items for which alarms are to be redirected via e-mail:

An engineer receives an Alarm Redirection e-mail.

To acknowledge the alarm remotely, the engineer replies to the e-mail. (If the system is configured to use an e-mail Acknowledgment Keyword, the engineer has to enter the keyword in the subject line of the reply (see E-Mail Settings). If the system is also configured to use an e-mail Hiding Keyword, the engineer would instead delete all, or part, of the Hiding Keyword from the body of the reply (see E-Mail Settings)).

When the server receives the e-mail (and, if applicable, that e-mail includes the appropriate Acknowledgment Keyword, and has part or all of the Hiding Keyword removed), Geo SCADA Expert checks whether the alarm is still in existence. If the alarm still exists and has not already been acknowledged, Geo SCADA Expert updates the alarm status to acknowledged by the user to which it sent the Alarm Redirection e-mail. The status change is logged with a comment indicating that the alarm was acknowledged by e-mail.

The comment is included in the Event Journal:

and can be viewed on the relevant Status Display:

Further Information

To see the type of content that a redirection e-mail might contain when the servers are configured to use an 'Acknowledgment Keyword' and a 'Hiding Keyword', see Use a Hiding Keyword to Acknowledge Alarms Remotely by E-Mail.