User-Specific Alarm-Related Preferences

This section summarizes the alarm-related options that a system administrator can configure on a per-user basis. The options apply to users that log onto the system using a User Account.

The options for each individual User Account, if they are to differ from the defaults, should be specified once that User Account has been added to the system.

For a user that logs onto the system using an individual User Account, use that user’s User Form to:

For information on configuring any of the above, see Creating a User Account in the Geo SCADA Expert Guide to Security. Also see Specify a Default Alarm Filter.