Enable or Disable EcoStruxure Web Services

Use the EcoStruxure Web Services tab on the Root Group Form to enable or disable EcoStruxure Web Services (EWS). When you enable EWS, you need to specify an EWS user account. You can then control the access that EWS clients have to the Geo SCADA Expert system, by defining the user account's security settings (see User Accounts).

The EWS user account that you specify applies to any EWS client that is used in conjunction with Geo SCADA Expert; it is not limited to the Geo SCADA Expert Advanced or Simple EcoStruxure Web Services Client Drivers.

To enable or disable EWS and create an EWS user account:

  1. Display the Root Group Form. To do this, right-click on the system in the Database Bar and select Edit Properties (see Configure the Properties of the Root or System Group).
  2. Select the EcoStruxure Web Services tab.

  3. Select the Enabled check box to enable EWS

    Or:

    Clear the check box to disable EWS (the default). If you disable EWS, clients will not be able to connect to EWS.

  4. If you enable EWS, you need to specify an EWS user account. To do this, select the browse button next to the User field.
    This displays a reference browse window.
  5. Use the Reference browse window to locate the user account you want to use.
  6. Select the user account.
  7. Select the OK button.
    This closes the Reference browse window. The name of the user account appears in the User field.
  8. Save the configuration.

To connect to EWS, use the URL: http://<server>/webservices/secorp