Database Bar

The Database Bar is an Explorer Bar (see Explorer Bars). It provides access to the database items to which the ViewX or Virtual ViewX client and your user account have access. The items are displayed in a hierarchical ‘tree’ structure that corresponds to the way in which your database is organized (see Working with Explorer Bars).

Database items are contained within groups that correspond to the Groups, Group Templates, and Group Instances that are configured in the database. You can expand individual groups to display their contents, or collapse them to hide their contents (see Working with Explorer Bars).


On a Virtual ViewX client, you can use the Database Bar to access operator-level displays and features in the database (see Working with Explorer Bars).

On a ViewX client, depending on your user account’s permissions, you can use the Database Bar to:

To perform any of the above on a ViewX client, right-click on the required item in the Database Bar to display a context-sensitive Object Menu. The menu will provide you with options (‘pick actions’) to view or modify the selected item. For information on the options that are common to many database items, see Object Menu Options. For information on the options that are common to driver-specific items, see Actions that are Common to Many Drivers.

An icon that displays a red cross in the Database Bar indicates an item that has invalid configuration (see Checking for Invalid Configuration).

Such an item will have a limited subset of menu options available from its context sensitive Object menu, as that item will not be ‘live’.

An icon that displays a red arrow in the Database Bar indicates an item that belongs to an instance of a group template (see Working with Explorer Bars).

A notification indicator next to a database entry indicates that a message for that item is available to configuration engineers in the Messages window.

See Diagnostic Messages and Notification Display.

Working with the Database Bar

This section summarizes the Database Bar interaction features that are available in addition to those that are supported by the other Explorer Bars.

Filter Entries in the Database Bar by Name

You can filter the entries in the Database Bar and Operator Documents Bar. For more information, see Filter the Entries in an Explorer Bar.

Perform Multi-Select Operations

You can select multiple database items simultaneously in the Database Bar if they are in the same group and level. To do this, use the SHIFT key and/or the CTRL key with the left mouse button. You can copy, move or delete these multiple selections as a single operation.

Drag-and-Drop Across Systems

If your User Account is assigned the relevant permissions, you can import database items into your Geo SCADA Expert database from a Geo SCADA Expert database on another system (see Import Database Items). You use a Geo SCADA Expert to import the configuration into your database.

If you drag-and-drop of one or more .sde files from another system into the Database Bar, this triggers an 'import merge' operation (rather than an 'import copy'). This is the same behavior as the Database Bar's Import context-sensitive menu command.

Choose the Monitor on which you want to Display or Edit a Document

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.