Naming Restrictions

When naming or renaming an item in Geo SCADA Expert, you have to take into account these restrictions:

Further Information

Restrictions that apply to the names of Mimic Parameters: see Add a Mimic Parameter in the Geo SCADA Expert Guide to Mimics.

Restrictions that apply to the names of parameters that you can use in Template expressions: see Template Parameters in the Geo SCADA Expert Guide to Expressions.

For examples that demonstrate using an ESCAPE clause in SQL queries, see the SQL Guide.