Preparation

With Geo SCADA Expert, you can:

For more information, see Database Structure.

As part of the preparation before adding an item to the database, you need to consider:

You might also want to consider using:

You also need to be familiar with the Basic Configuration Procedures and be logged onto the system as a user with the relevant permissions (see User Accounts).

Many of the items that you configure in the database represent the plant, measuring instruments or control devices that are on your system. As such, much of the configuration of those database items needs to correspond to the settings that exist on, or that are supported by, those devices. In order to configure the database items successfully, you need to be aware of those settings.

Taking each of the above into consideration, should enable you to add and configure items rapidly and successfully in the Geo SCADA Expert database (see Add an Item to the Database).