Configure General Ethernet Properties

SCADAPack E outstations are supplied with 1, 2 or 3 Ethernet interfaces. Use the fields within the Ethernet 1 and, if applicable, the Ethernet 2 and Ethernet 3 sections of the SCADAPack TCP/IP tab to define the general properties for the interface(s).

If the outstation does not have the Ethernet 2 and Ethernet 3 interfaces, the fields within those sections of the tab are ‘grayed out’ and unavailable for use. This is defined by the Outstation Type property (see Specify the Outstation Type).