In-Database Translation Dictionary Excel Add-In Program Options

The In-Database Translation Dictionary is part of the Geo SCADA Expert database and, for convenience, you can create and maintain it in a Microsoft® Excel® spreadsheet by using an Excel add-in program. For more information, see Introduction to the In-Database Translation Dictionary.

This section provides a reference to the In-Database Translation Dictionary Excel options, which are as follows: