Introduction to the In-Database Translation Dictionary

Intended Audience

This guide is designed for system administrators who are setting up and managing the Geo SCADA Expert In-Database Translation Dictionary.

Document Scope

The guide explains how to create and manage an In-Database Translation Dictionary.

About the In-Database Translation Dictionary

You can replace user-created text in Geo SCADA Expert with text translations. To do this, you create an In-Database Translation Dictionary which contains the user-created text and associated translated text. You then mark the user-created text in Geo SCADA Expert that you want to replace and Geo SCADA Expert will perform a search and replace using the In-Database Translation Dictionary.

For example, you might want to replace text in a Mimic with a translation of the text in another language. In Geo SCADA Expert, you mark the text you want to replace with a @ prefix. Geo SCADA Expert will then search for the marked text in the dictionary, retrieve the translated text associated with it, and then replace the marked text with the translated text.

You can use the In-Database Translation Dictionary in the following:

You can create two types of Translation Dictionary in Geo SCADA Expert: a File Translation Dictionary and an In-Database Translation Dictionary. You can use either of them to perform the search and replace for marked text. However, you can only enable one type of dictionary for use at a time. This guide describes the In-Database Translation Dictionary, which is the type of translation dictionary that we recommend you use

If you want to know more about the File Translation Dictionary, and why you might want to use it, see Introduction to the Geo SCADA Expert Translation Dictionary.

Some of the advantages of using the In-Database Translation Dictionary are:

For information on installing the Excel add-in program, .

Before you can create or update an In-Database Translation Dictionary, you must first:

This guide describes how to create and update an In-Database Translation Dictionary by using a Microsoft® Excel® spreadsheet.