Work with Common List Options

Geo SCADA Expert provides you with a set of common List options that allow you to change how the information on a List is displayed. When you display a List, you can right-click on an entry in order to display a context-sensitive menu. You then select the menu option that you require:

With Alarms Lists, Events Lists, and Queries Lists, the following options might also be available:

(There are restrictions as to when the 2 options appear on Events Lists - click on the links above for information.)

 

When a query is actually running, you can also cancel that query (see Cancel a Query).