Disable Device
Associated with: Sparkplug™ Device items
Security permission required to access this pick action: Disable Points
NOTE: The 'Disable...' series of pick actions are assigned the Disable Points security permission so that users with that permission can disable database items without necessarily being given the full Configure security permission. A user, such as an operator, whose User Account is given the Disable Points permission but not the Configure permission can disable a database item, but is prevented from altering the rest of that item's configuration.
Use this pick action to take a Sparkplug Device item Out of Service.
The Disable Device pick action clears the Device's In Service property, so that the Device is no longer active.
You might want to disable a Device database item, for example, if Geo SCADA Expert has detected a problem with the publishing device that the database item represents. Once the problem has been rectified, use the Enable Device pick action to place the Device back In Service.
Geo SCADA Expert logs an entry in the Event Journal whenever either pick action is used. The entry indicates whether the Device has been enabled or disabled.
Be aware that disabling a Sparkplug Device also de-activates its dependants, although their configuration will remain unchanged. Dependants include items such as points that are associated with the Device.
When the Device is disabled, Geo SCADA Expert ignores any messages that it receives from that device.
If using this pick action with the Automation Interface, you need to specify the method name Disable.