Enable Device

Associated with: Sparkplug™ Device items

Security permission required to access this pick action: Disable Points

Use this pick action to place a Sparkplug Device item In Service. Triggering the action changes the Device's configuration so that its In Service property is enabled and the Device becomes active.

When the Device item is enabled, Geo SCADA Expert processes any messages that it receives from that device. This occurs providing that the Broker, Group, EoN Node, and Device database items are In Service and have valid, saved, configuration, and Geo SCADA Expert is able to connect successfully to the broker.

The Enable Device pick action is only available for a Sparkplug Device:

  • That is not In Service
  • For which your User Account is allocated the Disable Points security permission.

Also see Disable Device.

If using this pick action with the Automation Interface, you need to specify the method name Enable.