Display the Parameters Window

You need to access the Parameters window if you want to add, edit, or remove a Mimic parameter.

To display the Parameters Window:

  1. Display a Mimic in Design mode.
  2. Select the Graphics tab on the ViewX ribbon.

  3. In the View command group, select Parameters.

    The Parameters window is displayed.

The Parameters window lists Mimic parameters (if any have been configured) under these headings:

The Parameters window contains these buttons:

There is a Test Value field that you can use to check that the parameter is working as you expected. You can enter a suitable value in the field to see how the parameter will use the value. The settings that you enter in the Test Value field are purely for test purposes—they are not stored.

 

If you have set up a Mimic parameter that uses a color value, when you enter a valid number in the Test Value field, the Mimic item that is associated with the parameter should change to the appropriate color. (For a color value, a valid number is in the range 0-255 inclusive.) The color that is displayed depends on the colors and value ranges that are defined for that particular property on the database item.