Configure Digital Points

Use an OPC UA Digital Point to map an item of data on an OPC UA server to a digital point in Geo SCADA Expert database. You do this when the item of data on the OPC UA server has a digital value, to enable Geo SCADA Expert to represent that data in the database.

You configure the properties of each digital point using fields on the OPC UA Digital Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

The Digital Point tab includes properties that are specific to OPC UA Digital Points.

Use the Digital Point tab to:

With each digital point that is to operate as an output point (in order to control plant), you also have to enable and configure the properties on the Control tab. You also use the Control tab to:

With an output point, users with the relevant security permissions can use either the 'standard' Control pick action, or the Control VQT pick action to write point data to the OPC UA server. (The latter provides the ability to write additional properties (the Quality and/or Timestamp) to the OPC UA server.)

Further Information

Minimum Configuration - Points.