Configure Time Points

Use an OPC UA Time Point to map an item of data on an OPC UA server to a time point in Geo SCADA Expert database. You do this when the item of data on the OPC UA server has a time value, to enable Geo SCADA Expert to represent that data in the database.

You configure the properties of each time point using fields on the OPC UA Time Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

The Time Point tab includes properties that are specific to OPC UA Time Points.

Use the Time Point tab to:

Further Information

Minimum Configuration - Points.