Add and Configure the Entries in an Edge Firewall Table

The Edge Firewall Table is only available on a SCADAPack 47xi device.

This topic only applies to SCADAPack x70 devices on which the Enable Edge Firewall check box is selected (see Enable or Disable the Edge Firewall).

You use a SCADAPack x70 Edge Firewall Table to specify the addresses and services from which a particular SCADAPack x70 device is to accept inward network traffic, when that SCADAPack x70 device connects to the Edge Applications platform under Linux (see Port Function - Edge). When the Edge Firewall is enabled (see above), only network traffic that is transmitted from addresses and services that are included in the Edge Firewall Table is accepted; network traffic that is transmitted from addresses and services that are not included in the Edge Firewall Table is ignored.

You use the table to specify the IP addresses and other parameters of permitted IP network traffic. You need to add an entry for each non-local IP address from which the SCADAPack x70 device is permitted to accept data.

WARNING

communication loss

Omission of IP addresses that are used by Geo SCADA Expert can lead to loss of communication between Geo SCADA Expert and your SCADAPack x70 device. Similarly, omission of IP addresses that are used by other devices with which the SCADAPack x70 device is expected to communicate can lead to loss of communication between the SCADAPack x70 device and those devices.
Verify that the required IP addresses are included in the Edge Firewall Table and that the specified settings are valid for the device and your network.
Failure to follow these instructions can result in death or serious injury.

The entries that you specify in an Edge Firewall Table are persistent (that is, they are retained when the SCADAPack x70 device restarts).

In the Geo SCADA Expert database, the table is built into the SCADAPack x70 Device Configuration item to which it relates. Changes made to the firewall configuration are downloaded to the SCADAPack x70 device when that device's Download Configuration pick action is next executed.

If you are to add or edit an IP Address on a SCADAPack x70 device that connects to the Edge Applications platform under Linux, you have to enable the Edge Firewall.

You can enable or disable the Edge Firewall using either of the following options:

  • Use the Enable Edge Firewall check box on the Edge Firewall Table tab on the SCADAPack x70 Device Configuration item's tables.
  • Use the Enabled check box in the Edge Firewall section on the IP Communications tab on the Form of the SCADAPack x70 Device Configuration item (see Enable or Disable the Edge Firewall).

By design, each of these options is in sync with the other. (If the configuration Form is open when the check box's setting is changed on the Table, you might have to close and then re-open the configuration Form in order for the check box on that Form to display its inherited value. Likewise, if the check box's setting is changed on the configuration Form while the Table remains open, you might have to close and then re-open the Table in order for the check box on that Table to display its inherited value.)

 

You specify these properties for each entry in a SCADAPack x70 Edge Firewall Table:

IP Address

The IP address of the source of permitted network traffic. This could be the IP address of a device, a monitor PC, or another address. Use the IP Address in conjunction with the Subnet Mask to identify either a single source address, or a range of source IP addresses.

The valid format is nnn.nnn.nnn.nnn. Omit any leading zeros from the address.

 

192.168.0.1

Subnet Mask

Used in conjunction with the IP Address to identify either a single source address, or one of a range of source addresses (a subnet) to which the SCADAPack x70 device is permitted to receive TCP/IP packets.

The valid format is nnn.nnn.nnn.nnn. Omit any leading zeros from the address.

 

255.255.255.255

Description

Short descriptive text used to identify the entry. The maximum length is 64 characters.

Traffic Direction

The direction(s) in which traffic is permitted for this IP address.

When adding or editing an entry in the table, you use a combo box to select the required direction. The options are Inbound and Outbound, Inbound, and Outbound. The default is Inbound and Outbound.

Port Number

This property only applies when the Permitted Services (see below) is set to 'Custom Service'. The property is used to specify a custom Port Number via which IP traffic is permitted. The Port Number has to be in the range 0 to 65535 inclusive.

Protocol

This property only applies when the Permitted Services (see below) is set to 'Custom Service'. The property is used to specify the data transmission protocol via which network traffic is permitted.

When adding or editing an entry in the table, you use a combo box to select the required protocol. The options are TCP, UDP, and TCP and UDP. The default is TCP.

Permitted Services

Used to specify the service(s) for which traffic is permitted for this particular IP address. At least one option has to be selected. The options are:

  • DNP3 over TCP
  • DNP3 over UDP
  • Modbus/TCP
  • Modbus RTU over TCP
  • Modbus RTU over UDP
  • Logic Debug Service
  • Telnet
  • FTP
  • HART Pass Through
  • IEC 60870-5-104
  • Terminal Server for Serial Port 1
  • Terminal Server for Serial Port 2
  • Terminal Server for Serial Port 3
  • Terminal Server for Serial Port 4
  • ICMP Ping Traffic
  • All ICMP Traffic
  • HTTPS Secure Web Server
  • SSH
  • NTP
  • Custom Service.

The options that are available for selection vary, depending on the model of SCADAPack x70 device and the configuration of its ports (see Device Configuration Serial Port Tabs and see Device Configuration IP Communications Tab). Options that are not applicable are 'grayed out' and unavailable for use.

With the ICMP options, 'ICMP Ping Traffic' only permits ping traffic via the specified IP address, whereas 'All ICMP Traffic' permits all ICMP traffic via that IP address, including ping traffic.

Use the 'Custom Service' option if you want to specify a custom Port Number and transmission Protocol for which network traffic is to be permitted from a particular IP address.