Define the General Modbus Point Scanner Properties
This topic only applies to systems on which SCADAPack x70 Modbus Point Scanners have been created manually (see Configure Modbus Point Scanners Settings).
These properties are included at the top of the Modbus tab on the configuration Form of a SCADAPack x70 Modbus Point Scanner:
Use to specify whether the Modbus Point Scanner is 'In Service' and included in the downloaded/exported configuration (see The 'In Service' Check Box and Items Taken Out of Service).
Use to specify the Modbus Server Device with which the point scanner is associated.
Use the browse button to display a Reference browse window and then select the required entry from the window.