Remove Logic Application

Associated with: SCADAPack x70 Device Configuration items

Security permission required to access this pick action: Control

Use the Remove Logic Application pick action to remove the local copy of the SCADAPack x70 logic application that exists for the SCADAPack x70 device in Geo SCADA Expert. A SCADAPack x70 logic application might exist in Geo SCADA Expert if:

  • It has already been imported into Geo SCADA Expert from RemoteConnect (using the Import from RemoteConnect pick action)
  • It has already been uploaded into Geo SCADA Expert from the SCADAPack x70 device (using the Upload Configuration pick action).

To identify if a SCADAPack x70 Device Configuration item has a SCADAPack x70 logic application, view that item's SCADAPack Import File n status attributes. Files with the names "logicapp1.sta", "logicapp1.sig" and "station.apx" collectively define a logic application. For more information about such files, see the documentation provided with SCADAPack RemoteConnect software.

When you use the Remove Logic Application pick action, a confirmation dialog box is displayed (see Action Requests that Require Confirmation). The confirmation dialog box is displayed regardless of the settings used to determine whether similar confirmation dialog boxes are displayed for other types of pick actions.

After you remove the existing SCADAPack x70 logic application from the SCADAPack x70 device, if you intend to download configuration to the SCADAPack x70 device in future, you must import or upload a relevant replacement for the removed SCADAPack x70 logic application. You cannot download configuration to the SCADAPack x70 device, if the configuration does not include a SCADAPack x70 logic application.

If using this pick action with the Automation Interface, you need to specify the method name RemoveRTZ.