Specify the Data Logging Requirements - Analog Configuration

The SCADAPack x70 tab on the Forms of SCADAPack x70 Analog Configuration items contains a Data Logging section. Use the section to specify the data log and the required events that are to be logged for the SCADAPack x70 Analog Configuration item. The properties in the section are only available for use if the SCADAPack x70 Device Configuration item with which the Analog Configuration item is associated has Data Logging enabled (see Configure the Device Options).

Use the following settings:

  • Data Log—Specify the Data Log database item that defines the location at which Geo SCADA Expert is to store the logged events for this SCADAPack x70 Analog Configuration item. Use the browse button to display a Reference browse window and then select the required entry from the window.
  • Selected Events—Select the events that are to be logged for the SCADAPack x70 Analog Configuration item. For information about the features to which the events relate, see Set up Analog Configuration.