Specify the Data Logging Requirements - Counter Configuration

The SCADAPack x70 tab on the Forms of SCADAPack x70 Counter Configuration items contains a Data Logging section. Use the section to specify the data log and the required events that are to be logged for the SCADAPack x70 Counter Configuration item. The properties in the section are only available for use if the SCADAPack x70 Device Configuration item with which the Counter Configuration item is associated has Data Logging enabled (see Configure the Device Options).

Use the following settings:

  • Data Log—Specify the Data Log database item that defines the location at which Geo SCADA Expert is to store the logged events for this SCADAPack x70 Counter Configuration item. Use the browse button to display a Reference browse window and then select the required entry from the window.
  • Selected Events—Select the events that are to be logged for the SCADAPack x70 Counter Configuration item. For information about the features to which the events relate, see Set up Counter Configuration.