Security

The Security permission defines whether the User or User Group can access and alter the security settings of the selected item. The Security permission is used in conjunction with the Configure permission. When working with security-related database items (such as User Accounts, User Patterns, User Groups, User Rosters, and Password Blocklists), and Groups that contain any of those security-related database items, the following rules apply:

These rules also apply to Groups that contain security-related database items.

Availability: Is available to any User or User Group with the Security permission for the selected item. The Security permission cannot be restricted (you can only stop Users and User Groups from having access to the security settings by denying them the Security permission for database items on a per item basis).

NOTICE

SECURITY THREAT

On systems on which Geo SCADA Expert can Create users automatically from group membership, the incorrect assignment of security permissions on User Patterns and User Groups can compromise the security of the system. Always restrict the security permissions that are allocated to User Patterns, and to User Groups that are integrated with Windows domain groups or LDAP user groups. Only assign those permissions that are actually required, to help prevent the automatic creation of new user accounts that allow Windows or LDAP users to perform high-level tasks, such as shutting down the server.
Failure to follow these instructions can result in equipment damage.