Using the Default, Non-Trusted Certificate

ATTENTION: This section and associated topics apply to the Original WebX client only.

This topic relates to the HTTPS Support properties that are deprecated and provided as a fallback. The HTTPS Support properties will be removed in a future version of this product.

For improved security, instead of using the settings that are configured in the HTTPS Support section, Original WebX clients are now expected to connect to an IIS reverse proxy which connects to the Listen Port (see Define the Listen Port Settings for Original WebX Clients).

We recommend that you obtain a trusted certificate for use with Original WebX, as trusted certificates offer better protection against unauthorized system access. However, it is possible to use the non-trusted certificate that is generated automatically by Geo SCADA Expert.

You can either:

For more information, see the Geo SCADA Expert Knowledge Base.

NOTICE

SECURITY THREAT

Using a non-trusted certificate could compromise your system security. Installing a non-trusted certificate could compromise your system security. Potentially, it could lead to unauthorized access. For this reason, we strongly recommend that you use a trusted certificate.
Failure to follow these instructions can result in equipment damage.

Non-trusted certificates should only be used if a trusted certificate is not available and your business network is secure. (Although we still recommend that you use trusted certificates, even with secure networks).

If you use a non-trusted certificate, logging on via an Original WebX client will result in:

Or: