Define whether the Self-Signed Certificate Warning is Shown in Original WebX

ATTENTION: This section and associated topics apply to the Original WebX client only.

This topic relates to the HTTPS Support properties that are deprecated and provided as a fallback. The HTTPS Support properties will be removed in a future version of this product.

For improved security, instead of using the settings that are configured in the HTTPS Support section, Original WebX clients are now expected to connect to an IIS reverse proxy which connects to the Listen Port (see Define the Listen Port Settings for Original WebX Clients).

We recommend that you only use trusted certificates for Geo SCADA Expert and Original WebX connections as they provide a higher level of security. But if you are confident that your network is secure from unauthorized access, you may choose to use a non-trusted certificate (and acknowledge the lower level of security that a non-trusted certificate provides).

If you choose to use a non-trusted certificate, Microsoft Edge in Internet Explorer mode can display a warning message on Original WebX clients. The message informs the user that the certificate is not trusted and so may expose your system to security risks (see Using the Default, Non-Trusted Certificate).

This message can become annoying as it appears each time a user logs on to Original WebX. By using the Warn on Self-Signed Certificate setting, you can control whether the warning message is displayed.

To define whether the self-signed certificate warning is shown in Original WebX:

  1. Display the Server Configuration Tool and log on if required.
  2. Expand the System Configuration branch of the tree-structure.
  3. Select the WebX entry.

  4. In the deprecated HTTPS Support section, use the Warn on Self-Signed Certificate check box to define whether the warning message is displayed in Microsoft Edge in Internet Explorer mode:
    • Select the check box to allow the browser to display the message. Each time a user logs on to Original WebX, the message is displayed (if a non-trusted certificate is being used).
    • Clear the check box to prevent the browser from displaying the message. When users log on to Original WebX, there is no error message displayed, even if a non-trusted certificate is being used.
  5. Use the Warn on weakly signed certificate check box to define whether a warning message is displayed if the certificate encryption strength is below 2048 bits.
  6. Apply the changes to the server.