Server License Settings - Geo SCADA Expert
Each Geo SCADA Expert system requires a Geo SCADA Expert server license that defines which drivers are available, the number of database points permitted, the number of client commendations permitted, and so on.
Depending on the configuration of your system, each ViewX client might also need a license.
If you are using virtualization, you must acquire a separate license for each copy of Geo SCADA Expert that runs on a virtual server (see Virtualization and Cloud).
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Further Information
License your Virtual ViewX Installation.
License requirements for Geo SCADA Mobile: see the separate Geo SCADA Mobile documentation suite.