Comms Threads

The Comms Threads category provides status information about the threads that are handling the server-client connections.

The status information for each comms thread is categorized under these headings:

  • Id—A unique number that Geo SCADA Expert allocates and uses to identify the thread.
  • Thread Id—A unique number that the operating system allocates and uses to identify the thread.
  • Thread Id (Hex)—The ThreadId number in hexadecimal format.
  • Parent Link Count—Indicates the number of Comms Parent Links that the thread services.