PCS Tags
This section is only available in the tool if the PCS driver is installed. The driver is only available for installation if the relevant prerequisite components are installed on the Geo SCADA Expert server (see Geo SCADA Expert Prerequisite Components).
The Server branch of the Server Status Tool includes a PCS Tags category. This category provides status information about the tags that are subscribed to from the database items on this Geo SCADA Expert server.
NOTE: An OPC UA client or server can also use the PCS Service to subscribe to database items in the Geo SCADA Expert database.
The PCS Tags category displays the following information about each tag:
- Object Id—Indicates the identifying number of the subscribed Geo SCADA Expert database item.
- Tag—Indicates the tag that is subscribed to from the database item.