Geo SCADA Expert Prerequisite Components

The Geo SCADA Expert Installer will offer various prerequisites prior to the main installation activity. Some of these prerequisites are mandatory; others are optional and, when selected, permit additional features to be used. The prerequisite components comprise a combination of the following:
(The actual options that are offered vary, depending on the operating system and whether any of the components are already installed. For example, the Microsoft .NET Framework 4.8 is not offered on operating systems on which that component is already built in.)

WARNING

DO NOT UNINSTALL PREREQUISITE COMPONENTS

Uninstalling the prerequisite components may result in Geo SCADA Expert being unable to provide access to certain features, or being unable to run. It could also affect system security. For these reasons, do not uninstall the prerequisite components.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When you install Geo SCADA Expert, the components that are essential for Geo SCADA Expert to run on your operating system are installed automatically. A prompt is displayed for non-essential components, allowing you to choose the components that are relevant to your system.

We recommend that you only install components that you need for your system. For example, you only need to install:

Installing components that are not needed on your system uses up disk space unnecessarily. It also increases the attack surface. For improved system security, you should avoid installing or running components that you do not require on your system.

Further Information

Installation of Prerequisites.

Prerequisites for machines on which Virtual ViewX is installed: see Virtual ViewX Server Prerequisite Components.