Making Changes to your Geo SCADA Expert Installation

You can make changes to your Geo SCADA Expert installation by using the Geo SCADA Expert installer. For example, you can install additional drivers (in accordance with your license agreement) or uninstall Geo SCADA Expert components that you do not require.

WARNING

COMPLETE LOSS OF CONFIGURATION

When setting up a main-standby system, make sure that you restart the servers in the correct order if objects are already configured in your database. Make sure that the server with objects already configured is started first and is running as main, then start the partner servers and allow them to synchronize with the main server.
Failure to follow these instructions can result in death, serious injury, or equipment damage. Failure to start the servers in the correct order can result in the complete loss of configuration from the system, requiring recovery from a backup.

To make changes to your Geo SCADA Expert installation:

  1. Shut down the Geo SCADA Expert server. (The installation process requires the server to be shut down.) For information on shutting down a server, see Stop the Geo SCADA Expert Server in the Geo SCADA Expert Guide to Server Administration.

  2. Run the Geo SCADA Expert installer. To do this, you can either:
    • Insert the Geo SCADA Expert DVD and select the Install Geo SCADA Expert option. The Geo SCADA Expert Installation wizard runs.

    Or:

    1. Use the Uninstall or Change a Program feature, available from the Control Panel in Windows®. (For information about accessing the Control Panel, please refer to the Windows help.)
    2. In the Control Panel, select Programs and Features.
    3. Select Geo SCADA Expert in the list. You will see that the menu options change and now include Change. Alternatively, you can right-click on Geo SCADA Expert in the list to display a context-sensitive menu that contains a Change option.
    4. Select Change to run the Geo SCADA Expert installation wizard.
  3. Select Next.
  4. Select Modify.

  5. Use the Custom Setup page to specify which components are to be installed or uninstalled. For more information on using the Custom Setup page, see Custom Setup.
  6. Select Next.
  7. Select Install.
    Geo SCADA Expert adds or removes the relevant components, depending on the selections that you made on the Custom Setup page.