Virtual ViewX Server Prerequisite Components
Virtual ViewX is supported by Geo SCADA Expert 2019 onwards. We strongly recommend that you install the Virtual ViewX server on a different machine to the Geo SCADA Expert server. This is to avoid potential performance issues due to the number of resources that each application uses.
If you do install Geo SCADA Expert and Virtual ViewX on the same machine, both applications must have the same version and build number. This is because the applications share some resources.
The Virtual ViewX server is designed to run on a computer that has certain other components installed. The components comprise a combination of the following:
- Visual C++ Redistributable for Visual Studio 2015-2022 x86
- .NET 4.8 Full Runtime
- IISSetup
- IIS URL Rewrite Module 2
- Microsoft Application Request Routing 3.0
- SAP Crystal Reports runtime engine for .NET Framework (32-bit)
- Sentinel System Driver Installer 7.6.1.
DO NOT UNINSTALL PREREQUISITE COMPONENTS
When you install Virtual ViewX, the components that are essential for Virtual ViewX to run on your operating system are installed automatically. A prompt is displayed for non-essential components, allowing you to choose the components that are relevant to your system.
We suggest that you only choose to install components that you need for your system.
Installing components that are not needed on your system uses up disk space unnecessarily.
The SAP Crystal Reports runtime components are NOT installed by default. If you intend to install them you must purchase a Crystal Reports runtime license for each server on which these components are to be operational (clients do not need a license to use the runtime components). For servers on which the runtime components are operational, the Crystal Reports runtime license is included with the Geo SCADA Expert Crystal Reports driver license. Please contact your Schneider sales representative for more information.
Install the 64-bit version of the SAP Crystal Reports Runtime Engine on Geo SCADA Expert server installations (to enable generating and exporting of reports). Install the 32-bit version of the SAP Crystal Reports Runtime Engine on ViewX clients and Virtual ViewX servers (to display reports). Please select both if you are to run Server and Clients on the same computer. As the runtime components are prerequisites, you have to select them before you continue further with the Geo SCADA Expert installation (this is handled automatically in the Virtual ViewX installer). For more information about the installation order, see the Installation section of the Geo SCADA Expert Guide to the Crystal Reports Driver.
If you intend using Crystal Reports on your system, you also need to install the Crystal Reports prerequisites and driver on any
Further Information
Prerequisites for machines on which Geo SCADA Expert is installed: see Geo SCADA Expert Prerequisite Components.