Copy Trend Data to the Clipboard

This section explains how to copy a Trend’s data to the clipboard. Users with the relevant permissions can also copy a Trend’s definition to the clipboard. For information on copying a Trend’s definition, see Base a TrendSpec Definition on the Definition of Another Ad Hoc Trend.

Copy and Paste limitations apply when you are using a Virtual ViewX client (see Use Copy and Paste in Virtual ViewX).

When you display a Trend, each trace displays values for the amount of time shown on the X-Axis. You can copy these values to your PC’s clipboard and then import them into any application that supports pasting from the clipboard, for example Microsoft® Word or Excel.

When using the copy data to clipboard feature, you need to be aware of the following:

When you copy historic data from a Trace to the clipboard, it is stored using Tab Separated Values and the following syntax:

Label<tab>Mode
Time<tab>Value
Time<tab>Value
Time<tab>Value

...and so on.

Where:

If you use the copy feature to copy multiple trace data to the clipboard, each trace’s information is separated by a double tab, for example:

Label<tab>Mode<tab><tab>Label<tab>Mode
Time<tab>Value<tab><tab>Time<tab>Value
Time<tab>Value<tab><tab>Time<tab>Value
Time<tab>Value<tab><tab>Time<tab>Value

...and so on.

 

To copy the data for a single trace to the clipboard:

  1. Right-click on the trace in the Trend key.
    A context-sensitive menu is displayed.

  2. Select the Copy to Clipboard option.
    If the trace is a raw data trace or a current data trace, the data for the trace is copied to the clipboard. This is unless the raw data trace is using a summary of the values rather than the actual raw values. If the trace is using a summary of the values, a summarized or aggregated representation of the data is copied to the clipboard.
    If the trace is a processed historic trace, a context-sensitive menu is displayed.

  3. Select either the Raw Data or Processed Data option. For more information on these types of data, see Raw Historic Data on Trends, and see Processed Historic Data on Trends.
    The data is copied to the clipboard.
    The Raw Data option is unavailable if the total number of values required for the interval on the trace exceeds the Marker Limit that has been configured for the trace.

 

To copy the data for all traces on a Trend to the clipboard:

  1. Select the Edit tab on the ViewX ribbon.
  2. Select the Copy command.
    The data for all of the traces is copied to the clipboard. The data for each trace is separated in the copied data by a blank line.

    For the raw historic data traces, the raw data is copied to the clipboard (unless the number of raw values for the trace exceeds the point limit).

    For processed historic data traces, the processed historic data is copied to the clipboard. Any raw values that are shown on the processed historic trace are not copied.

    You can now open a third-party application and paste the Geo SCADA Expert data.

You can use the Export command on the Edit tab, or the Export to File option from the context-sensitive menu to export the data for all of the traces. By default, the data is exported in 'Text (Tab delimited)' format.