Trend Trace

The Trace is a line that represents a point’s values over a period of time. You can configure a Trend to display one or more traces simultaneously.

Trace

The values that are represented by the trace are indicated by Trend Markers, and these are joined by the trace line. When you first add a trace to a Trend, Geo SCADA Expert chooses a color automatically. To make the Trend as easy to use as possible, Geo SCADA Expert will detect the color of the background and then choose one of 22 colors. (The 22 colors used are based on the results of Kenneth L Kelly's color research). However, these colors are only applied when you first create a trace.

If your User Account has the Configure permission, you can configure the trace to have a different source (the point that provides the values that are plotted on the Trend). You can also change the appearance of a trace, including its color, line style, and type of trace markers(see Configure a Trace).

There are two types of trace:

Pre-Configured Trends and ‘Custom’ Ad Hoc Trends are capable of displaying current and historic traces simultaneously. ‘Standard’ Ad Hoc Trends can only display current traces or historic traces—they cannot display both simultaneously.

When you view a Trend that has multiple traces, one of the traces will appear with more clarity than the others. This is because Geo SCADA Expert has a 'focus' feature that is designed to help improve your Trend viewing experience. By showing the currently selected trace in more clarity than the other traces, Geo SCADA Expert makes it easier to see the data on the Trend. This is particularly useful with Trends that contain several traces that have a high quantity of values.

Trend showing multiple traces, one with focus, others muted.

To change the focus, select one of the other Trends in the Key. The color of the selected trace will gradually become stronger and the other traces will appear to be faded out. The same effect is applied to the Y-Axes and Alarm Limits (those that apply to the selected trace are shown normally, whereas any other Y-Axes and Alarm Limits are faded out), see Define the Default Settings for New Trends.

When viewing a Trend, you can use the Hide Trace option to remove one or more traces from view (see Hide and Show a Trace). This is useful when there are multiple traces on the Trend and the amount of data on display makes it difficult to use the Trend.

Embedded Trends on Mimics provide a subset of the features that are available on pre-configured Trends. This includes operational-level access to a subset of the menu options on the Trend. Trends that have been configured to display in Inset Windows on Mimics support a slightly different subset of operational-level menu options to Embedded Trends.