Configuring a Trio Diagnostics Radio

The Simple Trio Diagnostics driver enables Geo SCADA Expert to communicate with a network of Trio radios, via one or more Trio ‘base’ radios. Each ‘base’ radio is connected to the Geo SCADA Expert server and provides the communications path to the other Trio radios on the radio network (see Supported System Setups).

You need to configure at least one Simple Trio Diagnostics Radio database item for each Trio radio from which Geo SCADA Expert is to retrieve diagnostics data.

If some diagnostics data needs retrieving more frequently than other diagnostics data on the same radio unit, configure two or more Simple Trio Diagnostics Radios to represent the same radio unit: one per required scan rate.

If multiple Trio Diagnostics Radio database items are to represent the same radio unit:

You specify the properties of each radio using the fields on the Simple Trio Diagnostics Radio Form. The Form has several tabs, including a Radio tab. The Radio tab contains radio-specific properties and properties that are common to Scanner database items on other simple drivers. For this reason, some of the references below refer to the ‘Configuring Scanners’ section in the Geo SCADA Expert Guide to Simple Drivers.

Use the fields on the Radio tab to:

 

The properties on the other tabs are common to many types of database item (see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers).