Operator Documents Bar

The Operator Documents Bar is an Explorer Bar (see Explorer Bars). It provides quick access to any of the operator document stores to which you have access. An operator document store is a special group that can be used to store documents, such as pre-configured Trends.

Each operator document store can be arranged using a hierarchical ‘tree’ structure (see Working with Explorer Bars).

For information on how to display the Operator Documents Bar, see Display an Explorer Bar.

For information on working with an Operator Document Store, see Operator Document Stores.