Introduction to the Advanced EWS Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is designed for use by engineers who are responsible for configuring EcoStruxure Web Services-specific items and features. It can also be used by system administrators when investigating any unexpected behavior relating to the Advanced EWS Driver. For more information, see EcoStruxure Web Services Specific Status Display Attributes and EcoStruxure Web Services Specific Driver Log File Options.

Document Scope

This guide explains how to configure Advanced EcoStruxure Web Services Client Driver specific features and items in the Geo SCADA Expert database. It also describes the Advanced EcoStruxure Web Services specific statistics and diagnostics.

ATTENTION: Throughout this guide, mentions of the 'Advanced EcoStruxure Web Services Client Driver' are abbreviated to 'Advanced EWS Driver.

The Advanced EcoStruxure Web Services Driver uses a Schneider-defined standard, which allows interoperability between Schneider products and devices. Geo SCADA Expert uses this standard to allow transfer of data between the Geo SCADA Expert server and other Schneider applications.

The Geo SCADA Expert Advanced EWS Driver is used to read and/or write to data on EWS servers, including:

The driver enables Geo SCADA Expert to communicate with servers that comply with EcoStruxure Web Services version 1.1.

For information about how to configure EWS specific features and items within the Geo SCADA Expert database (see Configuring EcoStruxure Web Services Devices in Geo SCADA Expert).

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).