Introduction to the Advanced Trio Diagnostics Driver
This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:
- Install and run the driver
- Ensure that the driver is licensed
- Configure the required database items and settings on the driver
- Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.
Intended Audience
This guide is designed for use by engineers who are responsible for configuring Advanced Trio Diagnostics features and items in the Geo SCADA Expert database. It can also be used by system administrators when investigating the cause of unexpected behavior relating to the Advanced Trio Diagnostics driver.
Document Scope
The Geo SCADA Expert Advanced Trio Diagnostics driver documentation explains how to configure Advanced Trio Diagnostics specific features and items in the Geo SCADA Expert database (see Configure the Server to Retrieve Trio Radio Diagnostics).
The guide also provides information about:
- Trio Diagnostics Terminology of which you might need to be aware.
-
Driver-specific aspects that may be of interest to system administrators and engineers when investigating unexpected system behavior (relating to the driver) (see Status Attributes that are Specific to the Advanced Trio Diagnostics Driver).
This guide contains technical information that is intended for users that are sufficiently familiar with Geo SCADA Expert configuration and operation. Before reading this driver guide, ensure that you are familiar with:
- Geo SCADA Expert configuration practices, procedures, and the configuration of properties that are common to many database items. For more information, see the Geo SCADA Expert Guide to Core Configuration, and the Geo SCADA Expert Guide to Core Point Configuration.
- Driver structure, components, and configuration properties, pick actions, and status attributes that are common to many drivers. For more information, see the Geo SCADA Expert Guide to Drivers.
- Advanced driver configuration order, outstation types, and configuration properties and logging options that are common to many advanced drivers. For more information, see the Geo SCADA Expert Guide to Advanced Drivers.
Geo SCADA Expert's Advanced Trio Diagnostics driver provides additional functionality to enable Geo SCADA Expert to communicate with a network of Trio radios. The driver enables Geo SCADA Expert to interrogate each Trio radio on the radio network for diagnostics data. The type of diagnostics data that Geo SCADA Expert can retrieve from each radio varies, depending on the radio series and the type of radio unit. Geo SCADA Expert can communicate directly or indirectly with a variety of Trio radio units across the radio network. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
For any Trio Diagnostics information not included in this guide, see the documentation supplied with your Trio radio equipment.
NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).
Policy of Continuous Development
To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).